Technical FAQs

Ask a Question

Will the I-Line II horizontal and vertical hanger assemblies accommodate All-thread as a hanging method?

Yes. All busway hangars are compatible with the use of 1/2`` all-thread.


CTA-ID : 2045253
Was this helpful?
What can we do to improve the information ?