Technical FAQs

Ask a Question

What is the coil burden for an LC type breaker with a 24VAC suffix 1042 shunt trip coil?

The coil burden for an LC breaker with a 1042 shunt trip is 30 VA with a maximum current of 1,250 milliamperes, or 1.2A.

CTA-ID : 2045092
Was this helpful?
What can we do to improve the information ?