Technical FAQs

Ask a Question

What are the voltage codes for LD* Integral starters?

LD*LB
18 amps 50 hz 60 hz
24 volts B BC
48 volts E ED
110 volts F K
120 volts . FC
220 volts M LC
240 volts U MC

LD*LC
32 amps 50 hz 60 hz
24 volts B BC
48 volts E D
110 volts F FC
120 volts . FC
220 volts M MC
240 volts U MC

LD*LD
63 amps 50 hz 60 hz
24 volts B BC
48 volts E CE
110 volts F K
120 volts . FC
220 volts M LC
240 volts U MC

A limited selection of DC voltages are also available.


 
Was this helpful?
What can we do to improve the information ?