Technical FAQs

Ask a Question

What is the dimension from the back of the enclosure to the tip of the handle on a DTU366, when in the OFF position?

The dimension is 13 7/8`` from rear of the enclosure to the tip of the handle, in the OFF position.


CTA-ID : 2045115
Was this helpful?
What can we do to improve the information ?