Technical FAQs

Ask a Question

Are the 9070T and 9070TF Control Transformer rated for 50 Hz?

Control Transformers are products that are used Worldwide, and must be able to be used on either of two geographically determined power frequencies

Product Line:
LV Transformers

Applies to all 9070 Class Control Transformer Products by SquareD/Schneider Electric

Power Systems Worldwide can be either 60 Hz or 50 Hz

All 9070 class CPTs are rated for 50 and 60 Hz

CTA-ID : 2045811

Was this helpful?
What can we do to improve the information ?