Technical FAQs

Ask a Question

What does the suffix P8 designate on the end of a 9007 limit switch?

The suffix P8 designates the addition of two LED pilot lights in parallel with normally open contacts.


CTA-ID : 2045294
Was this helpful?
What can we do to improve the information ?