Technical FAQs

Ask a Question

Can the ZBZ41 adapter that goes from a 30mm hole to a 22mm hole be used on any 22mm operator?

Issue:
Can the ZBZ41 adapter that goes from a 30mm hole to a 22mm hole be used on any 22mm operator?
Product Line:
ZB4 and ZB5 22mm Push Button/ 9001 30mm push button
Environment:
ZB4 and ZB5 22mm Push Button/ 9001 30mm push button
Cause:
Customer is trying to use 22mm operators in existing enclosure with 30mm knockouts.  
Resolution:
The ZBZ41 shrinks the cut out hole from 30mm to 22mm so any operator can be used.
 
Was this helpful?
What can we do to improve the information ?