Technical FAQs

Ask a Question

What are the dimensions for a MA1000S or MA1000F circuit breaker enclosure?

The MA1000S dimensions are 51.80`` high, 20.25``  wide, and 7.75`` deep. The MA1000F utilizes the same enclosure, but the cover is larger for the flush mount application. The flush cover is 52.60`` high, 21.84`` wide. Refer to drawing 3081, link provided below.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2045221
Was this helpful?
What can we do to improve the information ?