Technical FAQs

Ask a Question

Is the main bus of an UT2R2122B Horizontal Ganged Meter Socket rated for 205 amps?

Issue:
Application

Product Line:
Horizontal Meter Socket

Cause:
Clarification of rating

Resolution:
Yes, per UL414 Meter Sockets Table 24.1: Minimum allowable ampere rating for two meter sockets assembled together shall be 50% of the sum of both meter sockets added together, or 200A. The UT2R2122B was actually tested for a main bus rating of 205 amps.





CTA-ID : 2045058
Was this helpful?
What can we do to improve the information ?