Technical FAQs

Ask a Question

What are the repair parts for a PAK1004C, Series E02, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161 (2 req`d)
Interior Trim - 4054024801
Interior Trim Mounting Screw - 4020513001K (2 req`d)
Interior Assembly - 4054017351 (Includes the Circuit Breaker(s) and Receptacle(s) listed below. Also includes the neutral assembly, not listed separately. Does not include the Base Assembly listed below - order separately, if needed)
Interior Assembly Mounting Screw - 2142217101 (4 req`d)
Base Assembly - 4054008650
Base Assembly Insulator - 4054008501
Circuit Breaker - QO120GFI and (2) QO250
Receptacle - 4054001450 (125 volt/20 amp) and (2) 4054027950 (125/250 volt/50 amp)
Receptacle Mounting Screw - 2190312160 (1 req`d for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (2 req`d for each 125/250 volt/50 amp receptacle)
Neutral Bonding Strap Assembly - 4054017250
Ground Bar - 4023089990
Ground Bar Mounting Screw - 2159414200
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241 (2 req`d)
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 2045153
Was this helpful?
What can we do to improve the information ?