Technical FAQs

Ask a Question

On Circuit Breaker catalog number FA932030, what is the meaning of the ``9`` in the catalog number? Does it have copper lugs?

Yes. The ``9`` in the catalog number indicates that the breaker is marine duty rated. The Marine rating on a F frame breaker requires copper lugs.

CTA-ID : 2046156
Was this helpful?
What can we do to improve the information ?