Technical FAQs

Ask a Question

Can a FTL3200, fusible pullout be used on a 480Vac service?

Issue:
Product design feature

Product Line:
Fusible Pullouts

Environment:
Voltage rating

Cause:
Application

Resolution:
No, the maximum voltage system that a FTL3200 pullout can be used on is 240Vac MAX system.


CTA-ID : 2045131
Was this helpful?
What can we do to improve the information ?