Technical FAQs

Ask a Question

How do the operators match up with the contact blocks in an XALD, XALB or XALK control station?

The operator mounts in the cover of the control station, and the contact block mounts in the base. When the control station cover is assembled to the back box, the operators align with the base mounted contact blocks.


CTA-ID : 2045567
Was this helpful?
What can we do to improve the information ?