Technical FAQs

Ask a Question

How does a FAL34070 fit into a KA225S enclosure?

There are labels on the mounting pan that say FAL with an arrow pointing to a set of holes and KAL with an arrow pointing to a set of holes. The FAL breaker must be mounted in the correct holes on the mounting pan to compensate for the height difference in the two breakers. Also the mounting pan is adjustable. The customer will have to adjust the mounting pan foward so that the breaker is pushed forward toward the front of the box to compensate for the depth difference between the FAL and KAL breakers.

CTA-ID : 2045491
Was this helpful?
What can we do to improve the information ?