Technical FAQs

Ask a Question

Can a LAL36400 breaker be installed into a MA1000R enclosure?<br /><br />

Yes, it can. A mounting pan in the enclosure must be adjusted when using the LAL breaker.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2045691
Was this helpful?
What can we do to improve the information ?