Technical FAQs

Ask a Question

Do the 9007 snap switches have a NEMA or IP rating?

They do not have an NEMA enclosure rating, they are considered an open type device. They are not made to European standards and do not have an IP rating.


CTA-ID : 2045386
Was this helpful?
What can we do to improve the information ?