Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H365NR, Series E4 or E5 Heavy Duty safety switch?

Issue:
Product features

Product Line:
HD Safety Switch

Environment:
400A HD 

Cause:
Clarification

Resolution:
The lugs on this device will accept (1) #1/0 AWG - 750 kcmil or (2) #1/0 AWG - 300 kcmil aluminum or copper conductors per phase and neutral.
No optional lugs are available.


CTA-ID : 2045072
Was this helpful?
What can we do to improve the information ?