Technical FAQs

Ask a Question

What is the operating temperature range for the 9002AW2?

The operating temperature range for the 9002AW2 is -30 degrees C (-22F) to +60 degrees C (+140F).


CTA-ID : 2045069
Was this helpful?
What can we do to improve the information ?