Technical FAQs

Ask a Question

When we manufacture an NQOD factory assembled panel do we provide the specified number of branches and space only or do we provide the next larger interior?<br /><br />

We utilize the interior necessary to accommodate the breakers shown on the order. Breaker accessories that require an additional pole space are also taken into consideration when sizing an interior. We do not remove mounting fingers if they are not used or requested. However, branch connectors are removed or disabled in order to prevent a 42ckt rule violation in lighting panels.


CTA-ID : 2045822
Was this helpful?
What can we do to improve the information ?