Technical FAQs

Ask a Question

Can the main breaker in a SC816D200C be upgraded to achieve a rating of 22K AIC Short Circuit Current Rating?

This units UL Listed Short Circuit Current Rating is10K AIC maximum. It cannot be upgraded to 22K AIC.

CTA-ID : 2045714
Was this helpful?
What can we do to improve the information ?