Technical FAQs

Ask a Question

H365R and HU365R - Are the current carrying components in this device made of copper?

All current carrying parts are plated copper, with the exception of the lugs, which are plated aluminum. However, the lugs are suitable for use with either aluminum or copper conductors.

CTA-ID : 2045621
Was this helpful?
What can we do to improve the information ?