Technical FAQs

Ask a Question

Is a 12 circuit panel available in NQ type panelboards?

Issue: Is a 12 circuit panel available in NQ type panelboards? Product Line: panelboards. Environment: Products sold in the United States. Cause: Product features. Resolution: No. 18 circuits is the lowest number of circuits available in NQ panelboards. CTA-ID : 2045416
Was this helpful?
What can we do to improve the information ?