Technical FAQs

Ask a Question

What is the part number for a 600V arc suppressor, which is required to be used with a SS20 Additional Barrier Kit for 200A F-Series safety switches, when it is used on a 200A, 240V rated safety switch.?

Use Arc Suppressor Assembly - 40566-775-50.


CTA-ID : 2045391
Was this helpful?
What can we do to improve the information ?