Technical FAQs

Ask a Question

What are the repair parts for a QO13040M200K, Series S1, Load Center?<br /><br />

Only the parts listed below are considered field replaceable.
Cover - QOC30UF/S
Interior Assembly - QO13040M200I
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2200VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K
Door Latch Kit 4020284450K
Main Circuit Breaker and Main Lugs Keps Nut - 2342702001
Wiregator Inserts - 4055615301
Wiregator Wireguard Shields - 4055943550, QTY 2

CTA-ID : 2045322
Was this helpful?
What can we do to improve the information ?