Technical FAQs

Ask a Question

What is a QOU14100JBAR?

The QOU14100JBAR is a right-side-wired jumper bar assembly commonly used by OEM`s. The device is rated 100A, 240VAC maximum. A neutral is not included. It accepts (4) poles of QOU circuit breakers (1 or 2 pole only), 60A maximum. Each pole space must be filled. The device includes a base, cover, and mounting screw, but no enclosure. It carries a UR Component listing and a CSA listing.

CTA-ID : 2045309
Was this helpful?
What can we do to improve the information ?