Technical FAQs

Ask a Question

What is the recommended torque value for the PKOGTA2?

The wire binding screw needs to be torqued to 200 In./Lbs. The mounting screw should be torqued to 25-45 In./Lbs.


CTA-ID : 2046581
Was this helpful?
What can we do to improve the information ?