Technical FAQs

Ask a Question

Is it possible to get a single-barrel lug on the 480 V Multi-9 circuit breakers?

The single barrel lug is available for order on the Multi 9 C60 UL489 breakers using the ``SB`` suffix. The catalog numbers are all on Q2C and available for order.

CTA-ID : 2046492
Was this helpful?
What can we do to improve the information ?