Technical FAQs

Ask a Question

What is the coil tolerance for the Class 8501 type R relays?

AC coils are -15% to +10% of nominal voltage.
DC coils are -20% to +10% of nominal voltage.


CTA-ID : 2046527
Was this helpful?
What can we do to improve the information ?