Technical FAQs

Ask a Question

What is the continuous current rating of a 2510TCO3 starter ?

This is a NEMA rated device, size 1. It has a continuous current rating of 27 amps.


CTA-ID : 2046434
Was this helpful?
What can we do to improve the information ?