Technical FAQs

Ask a Question

Can the cover of a P1200R circuit breaker enclosure be padlocked closed?

Yes, the enclosure cover can be padlocked closed via a hasp located on the bottom endwall. There is also an integral circuit breaker access cover that can be padlocked closed.

CTA-ID : 2046421
Was this helpful?
What can we do to improve the information ?