Technical FAQs

Ask a Question

Can the operating handle of a P1200AWK circuit breaker enclosure be padlocked in the ON or OFF position?

The enclosed circuit breaker is operating via an external operating handle. The external operating handle can be padlocked in the OFF position only.

CTA-ID : 2046426
Was this helpful?
What can we do to improve the information ?