Technical FAQs

Ask a Question

Can the operating handle of a M800AWK circuit breaker enclosure be padlocked in the ON or OFF position?

The enclosed circuit breaker is operated via an external operating handle. The external operating handle can be padlocked in the OFF position only.

CTA-ID : 2046425
Was this helpful?
What can we do to improve the information ?