Technical FAQs

Ask a Question

Does Square D offer a 30 ampere non-fusible Air Conditioner Disconnect?

Issue:
Product selection

Product Line:
Air Conditioner Disconnect

Environment:
AC Disconnect

Cause:
Clarification

Resolution:
Non-fusible Air Conditioner Disconnects are available only in 60 ampere maximum. The QO200TR can be used for any amperage up to 60 ampere. The QO200TR is an enclosed molded case switch, 60A maximum, 240V, Type 3R. This is also available in a Type 3R non-metallic enclosure, catalog number QO200TRNM.


CTA-ID : 2046026
Was this helpful?
What can we do to improve the information ?