Technical FAQs

Ask a Question

What is a 14210?

Issue:  
Is there a weatherproof enclosure for flush mounting Multi 9 breakers in a wall or an enclosure?  

Product line:  
DIN rail mounted breakers

Environment:  
Multi 9 miniature circuit breakers

Resolution:  
The 14210 is a Multi Pole mounting kit consisting of a transparent hinged weatherproof cover.  The enclosure allows for up to 20 modules of the Multi 9 circuit breakers or supplementary protectors & accessories.  The Din Rail mounting support 14211 must be ordered separately if a DIN rail is not already in place to mount them to.  
Was this helpful?
What can we do to improve the information ?