Technical FAQs

Ask a Question

Customer needs a meter center rated 1600A, 208Y/120Vac , 3-Phase, 4-Wire having a SCCR rating of 100,000 RMS Symmetrical Amperes.

For this meter center, order Main device catalog number EZM32000CB1600, includes factory installed RJF36160
Branch units suitable for use with this main at the 100kA (208Y/120 Vac Maximum) level includes the following:
225A maximum Branch units with type QDP-TM tenant breakers ( 2-Pole or 3-Pole, 70A-225A), order breakers separately.
400A maximum Branch units supplied with factory installed type DJM tenant breaker(s) (2-Pole or 3-Pole, adjustable amp trip setting 160A-400A).


CTA-ID : 2045262
Was this helpful?
What can we do to improve the information ?