Technical FAQs

Ask a Question

Can the QO3HT be used on QOU breakers?

The three-pole handle tie will fit on the QOU, but the padlock attachment will not fit on the QOU Series 3 (low-amp frame). It would work on the QOU Series 1 in the 100-amp frame however.


CTA-ID : 2046264
Was this helpful?
What can we do to improve the information ?