Technical FAQs

Ask a Question

What sockets are used for type RSB Zelio Plug in Relays?

Socket with Separate Box lug connector for type RSB1A120** is part number RSZE1S35M.
Separate Box lug connector for type RSB1A160** and RSB2A080** is part
number RSZE1S48M. Note sockets are sold in lots of 10
When using the relay RSB1A160** with socket RSZ E1S48M, terminals 24 and 14, 21 and 11, and 22 and 12 must be jumpered.



CTA-ID : 2045012
Was this helpful?
What can we do to improve the information ?