Technical FAQs

Ask a Question

REVISION TO RESOLUTION 2030869<br />ADDED NOTES REGARDING REPLACEMENT TO EXISTING BUCKETS IN THE INQUIRY:<br />What is the plastic cover that swings out on an MCC model 6 that holds the Start/Stop pushbuttons, 22mm or 30mm

Advised customer that for the 22mm 5 device Control station panel, replacement part number is 80420-007-05. For the 30mm 3 device Station control panel, replacement part number is 80420-007-06. In either case the cover will be blank with perforated cut outs in the back. This a replacement part and cannot be added to an existing bucket that did not come set up to accept control devices.


CTA-ID : 2046443
Was this helpful?
What can we do to improve the information ?