Technical FAQs

Ask a Question

What are the phase barriers for the Powerpact M and P frame breakers, cat. no. S33646 made from?

The material is EPDM.(Ethylene Propylene Diene Monomere) and it is a EPR (Ethylene propylene rubber).

CTA-ID : 2046442
Was this helpful?
What can we do to improve the information ?