Technical FAQs

Ask a Question

Can the H and J Motor Circuit Protectors be used on single phase applications?

Yes, use any two poles for single phase application.


CTA-ID : 2046380
Was this helpful?
What can we do to improve the information ?