Technical FAQs

Ask a Question

What lugs are used for an EZM31200CBU?

No line side lugs are provided. The suffix ``U`` of the catalog number indicates that the device meets EUSERC standards. EUSERC requires factory supplied lug landing pads to accept field installed lugs. In EUSERC locations, the lugs will normally be supplied by the Utility Company. For contractor supplied lugs, the lugs should be ordered separately. Lugs listed for use on this device will be noted on the devices wiring diagram (located inside the front cover). You may also refer to CAD Drawing #3151 for a list of acceptable lugs or view the class 4100 catalog which are both available on the internet at www.squared.com.


CTA-ID : 2046394
Was this helpful?
What can we do to improve the information ?