Technical FAQs

Ask a Question

Will the QO and QOB breakers work at 12V DC?

Yes. The QO and QOB breakers are rated up to 48VDC. They may be used for DC voltages below this as well.

CTA-ID : 2046261
Was this helpful?
What can we do to improve the information ?