Technical FAQs

Ask a Question

Will the indicator lights on a DF103V three pole fuseholder work on AC or DC? What is the voltage level of the blown fuse indicator?

The blown fuse indicators use neon type lamps which are rated at 110-690V AC or DC.

CTA-ID : 2046355
Was this helpful?
What can we do to improve the information ?