Technical FAQs

Ask a Question

LC11021 has four terminals on it. Which ones are used for a 120V connection?

The LC11021 has the two terminals on the left and two terminals on the right. The sets on each side are connected internally. Connect to one of the terminals on the left and one terminal on the right side with the voltage supply.

CTA-ID : 2045926
Was this helpful?
What can we do to improve the information ?