Technical FAQs

Ask a Question

What is the ``F`` on catalog number 60224F?

This is a UL 489 Listed C60 Circuit Breaker with ring tongue terminals and a factory-installed fingersafe cover (IP20 per IEC EN60529).
The catalog numbers for these fingersafe products are the same standard C60 with ring-tongue terminals at both ends, but with addition of an ﾿F﾿ suffix (Example: 60204 would be 60204F).


CTA-ID : 2046341
Was this helpful?
What can we do to improve the information ?