Technical FAQs

Ask a Question

What are the differences between the 9999MB11 and 9999MB22?

With the 9999MB11 you have the choice of two or four wire Modbus. With the 9999MB22 you have two wire only. The MB22 can also power the small display, 9999MLPD.

CTA-ID : 2045031
Was this helpful?
What can we do to improve the information ?