Technical FAQs

Ask a Question

MA36600 and MAL 36600 - Will these breakers accept 700 kcmil conductors?<br />

The AL900MA standard lug will not. Need to order optional lug kit, AL800MA, which will accept (2) 500-750 kcmil. (One lug per kit, order three kits for each side of the breaker).


CTA-ID : 2046436
Was this helpful?
What can we do to improve the information ?