Technical FAQs

Ask a Question

What are the repair parts for an EZMR44125RHAB, Series 002 branch unit?

Only the parts listed below are considered field replaceable, and some components are no longer available:
Parts include Meter Socket through Tenant Circuit Breaker Compartment.
Quantities listed are for one position only (where part number only is given the order quantity for that part is one):

5-Jaw Meter Socket - 4052720650
Meter Socket Jaw Assembly - (4) 7329794850
Keps Nuts to secure Meter Socket Jaws - (4) 2342702001
Mounting Screws for Meter Socket - (2) 2159417121
Line Side Meter Socket Bus Connector, LEFT Side - 4052786950
Line Side Meter Socket Bus Connector, RIGHT Side - 4052786951
Keps Nuts for Line Side Bus Connectors - (2) 2342702001
Horn Bypass Connectors for LEFT Line and RIGHT Load Positions - (2) 4052783101
Horn Bypass Connectors for RIGHT Line and LEFT Load Positions - (2) 4052783102
Load Side Meter Socket Bus Connector, LEFT Side (Short) - 4052784501
Load Side Meter Socket Bus Connector, LEFT Side (Long) - 4052786250
Load Side Meter Socket Bus Connector, RIGHT Side (Short) - 4052786150
Load Side Meter Socket Bus Connector, RIGHT Side (Long) - 4052786350
Circuit Breaker Base Assembly - 4052788050
Mounting Screw for Circuit Breaker Base - 2196617201
Mounting Screws for Connector Fingers - (2) 2142717161
Fiber Barrier for Load Side meter socket bus connectors - (2) 4052780301
Pop Rivets for Fiber Barrier - (4) 2430313190

OTHER Available Parts for this device:
Cover Mounting Screw - 4020513002K
Equipment Ground Terminal Assembly - 4052737150
Mounting Screws for Equipment Ground - (2) 2142217101
Individual Meter Socket Trim (Ringless Type) - 4052790550
Gasket for Meter Socket Trim - 4052790550
Circuit Breaker RB Cover (one position) - BCV



CTA-ID : 2046244
Was this helpful?
What can we do to improve the information ?