Technical FAQs

Ask a Question

Do we offer a washer for the 4812422451 (48124-224-51)FAL circuit breaker mounting screws?

Because these screws are self-locking, no washer is provided nor is one needed. This bag of FAL breaker mounting hardware includes panhead slotted stee self-locking machine screws.


CTA-ID : 2046283
Was this helpful?
What can we do to improve the information ?