Technical FAQs

Ask a Question

What is the overall width of the enclosure for catalog number HU365AWK? Does the handle add to the overall width?

The width of the enclosure is 26.25``. The handle is located on the flange of the switch, so it does not add to the overall width dimension.


CTA-ID : 2045783
Was this helpful?
What can we do to improve the information ?